MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Brad Colbert Thanks very much. Documentation on how Librealsense uses CMake as a standard mechanism for building is available at the link below: https://github.com/IntelRealSense/librealsense/wik...
-
I have re-opened that case for further investigation.
-
The SR305 user in the case I mentioned earlier found that by editing one Librealsense file to disable CUDA in that file only, they could fix the broken depth. They created a forked version of the ...
-
In general, if Librealsense is being built from source then you have to deliberately enable CUDA support in the CMake build instruction, as it is False by default. If Librealsense is installed wit...
-
I am reminded of a case in the past week where somebody said that the 3D point cloud depth was not being displayed correctly if CUDA graphics mode was enabled. Do you know whether you have Nvidia ...
-
It is unusual that your SR305 is being detected as an SR300 but not necessarily bad. In fact, some people prefer getting their SR305 to be detected as an SR300 so that the camera works with old pr...
-
If your project budget allows it, you could add an Intel Neural Compute Stick 2 into a USB port alongside your RealSense camera for hardware acceleration of vision computing applications. The Stic...
-
If you want your application to follow only a ball and ignore everything else, object detection and coordinate reading using a Deep Neural Network (DNN) may work well for you. It can identify an o...
-
Have you ever run a driver installation program called the Depth Camera Manager or DCM since you bought your SR305?
-
At the top of the options side panel, is the name of the camera shown as 'SR300' instead of SR305, please? If it is, please go to the 'More' button just below the name and select from its drop-dow...