MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The RealSense Viewer and the Depth Quality Tool share the same design components, so a problem that affects one program can affect the other. Just to confirm that the problem is with these particu...
-
Let's try something different. Are you able to launch the Depth Quality Tool that also has a launch icon placed on the Windows desktop after installation of the Windows SDK, and successfully show...
-
Aeaa5023 It seems so. The firmware release notes for 5.12.5 state that "the release also includes support for 256x144 @ 300FPS and 848x100 @ 300FPS formats for D43x cameras".
-
The 400 Series cameras can become mis-calibrated if they receive knocks, which might have happened if the camera was in storage. High temperature may also cause mis-calibration. The 400 Series cam...
-
Are you using a recent firmware driver in your camera, please? If you have not upgraded the firmware inside the camera recently (or since you purchased the camera), you can do so by going to the ...
-
Can you get an image if you only activate one stream instead of two (depth only or RGB only)?
-
You do not need to install the Universal Windows Platform (UWP) driver unless you plan to use the 400 Series camera with hardware that supports UWP, such as the Microsoft HoloLens headset. Would ...
-
The SR300 was first released in 2016. The 400 Series released in 2018 used power more efficiently than the SR300, and that trend should continue with L515. The L515 is advanced technology that is ...
-
The SR300 was discontinued at one point, but got a second life when the RealSense SDK 2.0 was introduced. Then Intel introduced the SR305 model in 2019, which is an SR300 camera that is fully comp...
-
Thanks very much, I look forward to your test results.