MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Gutierrezjuanlucas It is fine to place a RealSense camera inside an enclosure with a clear transparent window on the front, like the custom enclosure for an underwater project in the image belo...
-
Hi Kevin No, there is not an error message when Inter Cam Sync Mode 2 captures unsynced after the wait period has elapsed.
-
Hi Leejonghak Although the D405 camera model is not equipped with the dot pattern projector that other RealSense models have to assist depth analysis of surfaces, the 400 Series cameras can altern...
-
Do you have access to a Windows 10 computer? If you do then are you able to perform calibration if you download the 2.49.0 version of the RealSense Viewer tool from the link below, please? 您可以使用 ...
-
Hi Mistahan Yes you can record from multiple cameras, though the recordings would be individual to each camera and not time-synchronized with each other. They will also be saved to individual .ba...
-
This question has been responded to at the link below. Thanks! https://support.intelrealsense.com/hc/en-us/community/posts/21313022125459
-
Hi Teamrobotica1 The D430i PID is supported by the RealSense SDK but not by the RealSense ROS wrapper. The D430i ID usually occurs with a D435i camera whose RGB sensor cannot be detected. If yo...
-
Hi Sjc6834 For some RealSense users the rs-convert tool does not generate .ply files but can generate other file types such as PNG images. It is a known issue and there is not a solution availabl...
-
Hi Gatordevin Yes, I can confirm that the FAKRA connection does not operate when the mode switch is set to USB, and the camera is detected and operates as D455 instead of D457. In USB mode it is ...
-
You are very welcome. Good luck!