MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
There was a past case of a RealSense user called Srikrishnan V who was also asking about bag files. Was that you, please? :) Anyway, in that case a RealSense tool called rosbag-inspector was men...
-
You are very welcome. Please feel free to post follow-up questions on this forum as you develop your project. Good luck!
-
Looking at how the light seems to be gathering within an indentation in the surface, I wonder if it may glare less if you push the affected surface outward so that it is not pushed-in.
-
It looks as though you have a strong light ray at the right-hand side of the image that is casting a powerful light on the side of the object and also producing strong light noise on the edge of th...
-
Although the D415 has better accuracy over distance, because the error curve increases linearly over distance from the camera there will be negligible difference in accuracy between the D415 and D4...
-
I also recalled a previous case in which the subject of measuring between two points had been discussed. https://github.com/IntelRealSense/librealsense/issues/6544
-
The RealSense SDK has a pre-made example program called Measure that automatically updates a measurement between two points of an object at the centerpoint of the camera's field of view. As the ca...
-
The L515 cameras support multi-camera hardware sync, yes. The RealSense SDK does also allow use of metadata to sync with streams from non-RealSense cameras (for example, depth from RealSense and R...
-
The RealSense 400 Series cameras have an error rate of 2% or less, and start at $149 for the RealSense D415 model. If you anticipate that your project will have fast camera movement or be tracking...
-
You are very welcome! A drone article was published on the official RealSense blog this week that should be a useful reference too: https://www.intelrealsense.com/everdrone/