MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
In a recent test that I did, I experienced an effect like this when using a Temporal Filter and setting its Alpha to a low value. The lower the value, the longer it took to update the image over t...
-
I recommend budgeting for 2W maximum power draw per camera, and the hub being able to supply 12W power. The USB standard allows up to 5 hubs to be linked together on a single computer. The averag...
-
Can you highlight which parts of the image are noise, please? Also, what filters are you using? Thanks,
-
I handle cases on both this forum and the GitHub, so I get around a lot. :) Look forward to the update!
-
As the SD card image provided was primarily intended to make it easier to test the open-source ethernet system in that guide, including OpenCV and Python in the build was probably felt to be unnece...
-
Intel have successfully tested the Amazon AmazonBasics powered USB 3 hub with a multicam setup in their multiple camera white paper document. On that recommendation, I bought the 7-port AmazonBasi...
-
I have personally only tested Cubemos with an Intel NUC 8 mini-PC but had no problems with it and have not heard reports of computing devices it will not work on. The free trial should allow you t...
-
If your preference is to use Python for person detection, there are programs based on MobileNet-SSD. https://github.com/IntelRealSense/librealsense/issues/3086#issuecomment-455181310 Intel also ha...
-
Intel have an official installation guide for Raspbian, though designed for Pi 3. https://github.com/IntelRealSense/librealsense/blob/master/doc/installation_raspbian.md Comparing the instruction...
-
Scott Stevens It sounds as though both situations may be caused by insufficient power available for all USB devices attached to the computer. So during boot, one of the devices may not get detect...