MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
-
You may not actually need the LED light. The camera can project IR light from its IR Emitter component to illuminate a scene even in dark conditions. The depth sensing can make use of that light,...
-
-
Hi Dhyoon The D457 camera model is able to use a USB cable by moving sideways a hidden physical switch under a removable cap on top of the camera. You could therefore power the D457 camera with a...
-
I note that all your images are of the 2.56.3 beta version of the Viewer. Does the freeze occur if you download and run the 2.55.1 version of the Intel.RealSense.Viewer.exe standalone Viewer? http...
-
Hi Allusrikanth87349 The 4 meter range limitation occurs because a post-processing filter called the Threshold filter is enabled by default in the 'Stereo Module > Post-Processing' section of the ...
-
Thanks very much for the clarification about how you are using the Viewer and DQT. Next, please try downloading the standalone executable version of RealSnse Viewer 2.56.3 by downloading and runn...
-
Because a bag file is a recording and is not accessing the camera sensors when it plays back, this could enable you to play the bag recording and stream live data in your program script at the same...
-
Thanks very much for the images. It is a positive sign that it can fully detect the cameras and display graphics before it stops responding. When a RealSense application starts streaming, it pla...
-
Hi Jnapoles Do they freeze if you launch them without any cameras attached? If they do still freeze without cameras present then it could indicate a problem with generating the graphics. If you...