MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Are there any strong light-sources projecting onto the wall that cause some areas of it to be illuminated brighter than other areas? A very strong light source cast onto the flat and low-textured ...
-
You can reduce the bag file size by using a lower resolution. For example, I recently did a test where I recorded a 10 second bag at 1280x720 and 848x480. The 1280x720 one was about 287 mb in siz...
-
Thank you very much. Does the wall look flat in the Viewer's 2D mode or is there a visible curving distortion in that mode too?
-
Hi Sonu Mathur87 The case in the link below has a similar example where a flat wall is rendered as curved. https://github.com/IntelRealSense/librealsense/issues/5435#issuecomment-622520372 A memb...
-
Thanks Jacob USB2 users should perform a firmware update through the RealSense Viewer program by going to the More option at the top of the Viewer's options side-panel. From there you can access...
-
The Failed to meet update rate error has also occurred in other cases where the D435i SLAM guide was being used. Here are a couple of examples: https://github.com/IntelRealSense/realsense-ros/iss...
-
Both Ubuntu 20.04 and Kernel 5.4 work with the RealSense SDK, though neither are officially validated to do so yet. Overall this combination seems to be relatively stable though in the months sinc...
-
Is it still the Python wrapper that is not detecting the camera please? And which model of 400 Series camera are you using? Thank you.
-
Hi Jiequanz The Cubemos Skeleton Tracking SDK is the product of a company called Cubemos, and they are responsible for providing support for it as the skeleton SDK is not an Intel product. To tal...
-
Hi Mhmh6086 If you experience problems with both of the above methods of building librealsense in Ubuntu then you could try a build method called RSUSB. It requires an internet connection to carr...