MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
If UWP driver 6.11.160.21 had been downloaded then there would likely be a folder called DMFT_Version 6.1.160.21 on your computer that contains a file called RS400Camera so that should make it much...
-
Thank you very much. If you are using Windows, do you remember if you have installed a program called the UWP Driver? If you have, and the driver is version number 6.11.160.21, then it should be ...
-
The most recent ROS2 Eloquent wrapper version at the time of writing this supports D455 and librealsense 2.38.1. https://github.com/IntelRealSense/realsense-ros/releases/tag/3.1.1 A comment by dor...
-
Hi Ayako Amma That ROS wrapper is on the main Intel GitHub site. It is a wrapper that is no longer updated and is not part of the RealSense ROS wrapper, which has its own dedicated GitHub. The R...
-
Hi Tcboy881118 As a starting point, could you first minimize the Laser Power option's slider to a very low level (not quite zero). If the disruption on the RGB image disappears then this would in...
-
Hi Amosz When trying to combine RealSense point clouds into a single cloud, a common recommendation is to perform an affine transform. Basically, just rotate and move the point clouds, in 3D spac...
-
I am not able to answer this question. Please start a new question on this help website so that another support team person can reply to it. **************** 私はこの質問に答えることができません。 別のサポートチームの担当者が回答でき...
-
Hi Mau. If you are testing the camera with the RealSense Viewer program, please go to its options side-panel, expand open the Stereo Module options and then expand open its Post-Processing sub-sect...
-
Hi Prparsons105 What you describe is a known issue with the RealSense Viewer on some computers. It can be worked around when programming in C++ or Python but I am not aware of a fix for the Viewe...
-
A way to test if the camera hardware is faulty is to configure it with the settings below. If you can receive an image in this mode then the camera hardware should be okay. Infrared 1280x800 25 FPS...