MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
In that particular case, the user experienced the error when replacing the Vision Processor D4 board inside a D435 camera with a new D4 board. So their camera would have been using the original RG...
-
Thank you very much for your tests. Does your project require a 3D pointcoud image or would a non-pointcloud aligned depth-RGB image like that from rs-align be sufficient? If you do require a po...
-
The RealSense Viewer's 3D pointcloud mode uses the same depth-RGB mapping method as rs-pointcloud. Could you open the Viewer please and click on the 3D option in the top-right corner of the Viewer...
-
There is not an existing documented case to refer to where there was a successful outcome reported when dealing with this Dynamic Calibration tool error. There are two main ways of performing dep...
-
Hi Yaser Jay This error has been encountered previously by a couple of other RealSense users. Guidance about the error written by Intel offers the advice below to attempt to correct the problem u...
-
You could use the save_single_frameset() instruction to save a single frame snapshot to a .bag format file. A bag is like a video recording of camera data that can be played back as though it is a...
-
A rare issue can occur where the depth sensor develops a No Frames Received failure after the camera has been stored inactive in a small space for weeks or months. This is a hardware fault and the...
-
Has there been a period of weeks or months before you discovered this problem when the camera has been stored unused in a space such as a cupboard or drawer, please?
-
I also note that you are using the High Accuracy visual preset. This may also be contributing to reduction of your image quality, as this setting tends to excessively strip depth detail from the i...
-
Any projector that adds some kind of texture or random dot pattern to a surface should be helpful for the camera's depth analysis. Yes, in the case of a random dot pattern, the more dots on the s...