MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
If you are using a 400 Series camera, a list of links relating to accessing video conferencing RGB with these camera models is below. It will hopefully be helpful reading. https://github.com/Intel...
-
Hi Fvmava. Which RealSense camera model are you using please? If you have an F200 or SR300 camera, these models have a built in audio microphone, so at the least you may be able to use it as a v...
-
Hi Ahughes FaceRig and the free RealSense-specific version IRFaceRig pre-date the launch of the RealSense 400 Series cameras at the end of 2017. It can be used with the original-generation RealSe...
-
Thanks very much for the files. Is the grid of squares applied as an overlay onto the images after they have been generated? In other words, it is not something that the camera sees. The empty sp...
-
NUCs can use Windows and Linux. The Mini PC models that are ready to run out of the box have Windows 10 pre-installed. https://www.intel.co.uk/content/www/uk/en/products/boards-kits/nuc/mini-pcs.h...
-
Hi Alessio Stella As RealSense 400 Series cameras can work with any Arm or Intel processor, any choice of industrial PC that has one of these processor brands should be able to work with your D415...
-
Hi @Jonathanfwade. The location of the drivers in the Device Manager is not an indication of a problem. The three SR300 drivers (RGB, Depth and Virtual) may be placed by Windows all under one cate...
-
Hi @F-nazaradeh You can set Windows to prevent automatic installation of updates. This can be used to prevent re-installation of an update that breaks a RealSense camera's functionality. My res...
-
Thanks very much for the additional information. The usual approach to having multiple RealSense cameras on the same port would be to use a USB hub. If the amount of space a hub would take up and...
-
Hi Ken Mccormack You can control camera sensors directly at the point of capture using the Low-Level API https://github.com/IntelRealSense/librealsense/blob/master/doc/api_arch.md The low level ca...