MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
An email contact is on the GitHub profile link above, under his name in the small side-panel.
-
Apologies for this next question, as it is important to consider all possibilities ... can you confirm that the powered USB hub is switched on at the mains electricity power point please?
-
The developer called lramati was the main programmer on the non-example core files of the MATLAB wrapper, including the mex related files, according to the GitHub details associated with the files....
-
If you do not have a mains electricity powered USB 3 hub to attach the camera to but you do have a device that can charge its battery on a USB cable (like a tablet), a power workaround method that ...
-
I managed to locate the multicam reset script that I mentioned earlier. https://community.intel.com/t5/Items-with-no-label/D435-streams-work-once-then-crash/m-p/499732#M6053
-
If you have 2 cameras plugged in right now then I would suggest testing hardware_reset() with only one plugged in. The simple version of the hardware_reset code will try to reset the first camera ...
-
You can automatically reset the camera from a script using the hardware_reset() instruction. It can be set up to trigger when certain logic conditions are met, such as more than 50% of the pixels ...
-
The image from the RealSense Viewer looks more correct, with the bottles, fiducial tag card and foreground rack bars appearing blue and the detail behind the bottles progressively shifting towards ...
-
Thanks very much for the useful images. I would expect the foreground near to the camera to be primarily colored blue. It looks as though the surfaces that may be having their distance mis-read as...
-
RealSense does have strong software support, though avatar facial morphing with a webcam has become sophisticated enough that dedicated face landmark tracking with a RealSense camera is no longer n...