MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Y SQ The D435 camera model uses the Omnivision OV2740 sensor for its RGB sensor. The table below has specifications for this sensor when used as the RGB sensor.
-
The driver can be used with computing devices other than Jetson Xavier / Orin and with other deserializer modules (as long as they have a Maxim deserializer component), but the customer needs to mo...
-
The RealSense MIPI driver should work with LI-GMSL2-IPX-DESER without having to modify the driver. This is the only commercially available deserializer module confirmed by the RealSense team to be...
-
The Maxim MAX9296 deserializer component inside the Leopard LI-GMSL2-IPX-DESER is compatible with the MAX9295A serializer built inside the D457.
-
Hi IACTICONTROL CTIcontrol The RealSense GMSL driver can be found here: https://github.com/IntelRealSense/realsense_mipi_platform_driver It can be used with Jetson Orin without having to modify ...
-
Hi Ahmed Khalid Farrag There has been no news about the Intel RealSense PT Metrics product since December 2024 and its official website is not accessible.
-
D435i can also be purchased from the official online RealSense Store which ships to Egypt, though this may involve the previously mentioned import fees and taxes. https://store.intelrealsense.com/b...
-
Hi Ahmed Khalid Farrag There are not official branches or partners in Egypt, though my research did locate a supplier called Makers Electronics in Alexandria, Egypt who offer the D435i. Purchasin...
-
Hi Damiatamani456 There is a new generation of RealSense camera product coming soon called the D555. Its new Image Signal Processor (ISP) technology enhances RGB with Geometric Distortion Correct...
-
I am not aware of a means to define a specific librealsense version that the ROS2 wrapper should use. In theory there should not be a 'built with 2.51.1, running with 2.55.1' situation if you fir...