MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Kirkpennock The C++ example program rs-hello-realsense, which prints as a non-graphical text value the distance to an object in the center of the camera's field of view, would likely fulfill yo...
-
Given that the Viewer and rs-capture both rely on OpenGL graphics, it may be worth updating your computer's graphics drivers to see if it improves performance.
-
The ASIC and Projector temperatures in the Viewer are somewhat high in the mid to late 30s. Is it as high as that when using depth or RGB on its own? Does the casing of the camera feel hot to the...
-
You are very welcome. Please do leave a comment when you are ready to resume. Good luck!
-
Thank you, I can see what you mean in the video. I see that you have all post-processing filters disabled in the video. Does enabling them by left-clicking on the red icon beside **Post-Processing...
-
How does it perform if you use 30 FPS instead of 15, please.
-
Hi Jeswinmp44 The D435 and D435i camera models have a smaller field of view on the color sensor than the depth sensor. This is intentional and not a bug or calibration problem. The 2D mode of the...
-
I am not part of RealSense ID product support. Could you post the above question as a new case on this forum please, including 'F455' in the message title, so that the appropriate RealSense team m...
-
Your English is very good, so don't worry. It would be difficult to remove the shoulders from the image using the RealSense Viewer tool as they are the same distance from the camera as the face. W...
-
I do not know how a D455 could be detected as an F450, as they are different types of product. The D455 is shown in the link below. Can you confirm please that this is what you own, and not an F4...