MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Thanks very much for the update. Did the PC stop forcibly rebooting after disabling the GLSL settings? When No Frames Received occurs, are you still able to get the camera to work if you reboot th...
-
Hi Osallam I believe that the basic formatting for launching a bag with this program is: python3 read_bag_example.py -i <bag path and filename> For example: python3 read_bag_example.py -i test.bag...
-
The computer being forcibly rebooted is rare but I have seen previous cases of it, like the one in the link below where it occurred when using the Viewer's 3D mode. https://github.com/IntelRealSens...
-
My research of Windows version 20H indicated that numerous RealSense users have been able to use their camera with that Windows version, so Windows may not be an important factor in this case. Can ...
-
Thanks very much for the confirmation of the reset method that you used. The other method, activated through the CustomRW tool that is packaged with the RealSense Dynamic Calibration tool, is call...
-
Hi Hayakawa T Ak The RealSense 400 Series cameras can be used outdoors and in day / night. In those severe weather conditions though you may need to create a custom protective housing for the cam...
-
I note that you tried a 'Factory Reset' of the camera. Which method did you use please - the Camera Data mode of the RealSense Viewer, or the CustomRW tool that is part of the Dynamic Calibration ...
-
Hi Kirkpennock If your preference is to not make use of ROS or RealSense-compatible external software platforms then the options available for obstacle avoidance may be limited. The links below ...
-
Hi Priyankap Information about use of RealSense 400 Series cameras with USB 2.0 can be found in the link below. https://www.intelrealsense.com/usb2-support-for-intel-realsense-technology/ The numb...
-
If you would like to access IMU data through the RealSense MATLAB wrapper then the link below provides advice about doing so. https://github.com/IntelRealSense/librealsense/issues/5648#issuecomment...