MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Eremteknoloji An explanation of this warning is provided in the RealSense ROS discussion linked to below. If you are not seeing negative effects in the performance of your ROS session when the...
-
A 1 meter Type-C USB cable (A to C) is supplied with the D455. The cable is two-way insertion on the end that plugs into the camera. Pages 84 and 85 of the current edition of the data sheet docume...
-
Hi Almannaika RealSense cameras are safe 'Class 1' laser products. This question about pregnancy was recently asked in the link below, so I hope that the information there will reassure you. http...
-
Hi Masoumiii The camera's laser safety mechanism in the firmware driver for the 400 Series camera models will shut off the projector's laser when its projector temperature is detected to have fall...
-
The RealSense SDK has a TensorFlow wrapper that can be used with Python. It provide a range of samples to try, starting with object detection and classification and progressing through to use of l...
-
Hi Kaustubh Joshi1997 Has the camera been detectable in the Viewer as a D435i before today, or has it been D430i from the first time that you used the camera please? Does going to the More option ...
-
The SDK's OpenCV example page states that samples can be converted to OpenCV 4 with minor code changes. If your problem with prototxt is related to the OpenCV version then I don't know how to alte...
-
Hi Chetankumar Ekzenrobotics The link below features a project for using a RealSense D435 camera with a URCap and robot arm. https://github.com/dti-research/ur-learning-shifting-for-grasping Alt...
-
It is no bother at all. There are references about solving this error at the link below. https://support.intelrealsense.com/hc/en-us/community/posts/1500001251202-Can-t-open-MobileNetSSD-deploy-pr...
-
Hi Gracex. When this error occurs on Raspberry Pi, a solution that can resolve it is to locate files with the extension .so that are created after the Python wrapper has been built from source code...