MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The design of the D401 module makes it more challenging to mount on its own than other depth module models. Whilst I am not personally aware of plans to release the D401 module for purchase separa...
-
The RealSense ROS wrapper's pointcloud is of an unordered format by default. This can be changed to an ordered pointcloud by setting pointcloud.ordered_pc to true in the ROS2 4.x wrapper. The diff...
-
If you installed the full SDK with the automated installer file Intel.RealSense.SDK-WIN10 then you should not need Visual Studio to run the examples, as launchable pre-built .exe files of the examp...
-
If there is a confidential aspect of your project that you cannot discuss on a public forum then please email me at the address below. martyx.grover@intel.com
-
Is the pointcloud able to be generated if you define a custom stream configuration with a low specification of 640x480 and 15 FPS for both depth and color like the ROS2 launch instruction below? ro...
-
As your CPU is apparently under high processing demand, the Resource temporarily unavailable type of control_transfer returned warning may suggest that the Pi's processor is having difficulty keepi...
-
Hi James Miller Are the control_transfer returned warnings appearing a small number of times and then stopping or are they generating continuously? If they are continuous then this can indicate th...
-
I am an Intel RealSense Support Engineer, so I can assist in trying to improve results with your D405 camera in your particular project scenario.
-
In the Viewer, the Motion Module typically continues functioning normally and providing gyro and accel data even after a Motion Module Failure error occurs and so it can be considered to be a small...
-
That's excellent news that you were successful after flashing the JetPack! In the link below, a RealSense user shared an instruction guide that they wrote for installing pyrealsense2 on a Jetson ...