MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
In a case at the link below, a RealSense user was trying to save the white-balance settings that were active when auto white-balance was enabled so that they could replicate the same image conditio...
-
rs-enumerate-devices -c provides extrinsics transforms for both directions (color to infrared, and infrared to color). For example, the values below are from a D455. As the calibration inform...
-
The D405 and its short baseline is designed to produce best accuracy at a very close range of 7 cm to 50 cm whilst the D435i and its longer baseline provides accuracy over a further distance, with ...
-
Hi Dfr At the link below, a RealSense user created a SLAM navigation guide for ROS for the RealSense D435i camera model that included mapping and localization with RTABMAP, plotting trajectory and...
-
Hi Nguyenduyduc14 The RealSense camera model comparison guide at the link below states that the D455 model has an accuracy of <2% at 4 meters. https://www.intelrealsense.com/compare-depth-cameras/...
-
Hi Sergio Delgado Heras To run the script measure_new.py you need to have installed the RealSense SDK's Python compatibility wrapper pyrealsense2. As a starting point in investigating your case, c...
-
Hi Kota Mogami Reports of MIPI errors occurring are highly rare (with left MIPI errors even rarer than right ones) and so there is insufficient data to establish a pattern regarding whether their o...
-
There are a couple of GStreamer compatibility plugins for RealSense cameras at the links below. WKDSMRT https://github.com/WKDSMRT/realsense-gstreamer Aivero https://www.aivero.com/2020/03/gstreame...
-
Hi Mcui I do not have information regarding when the flexible HSF cables will be back in stock in the RealSense Store at the time of writing this. The cables are also stocked by FRAMOS though. ht...
-
Hi Dwiki74 The Cubemos Skeleton Tracking SDK software was a product of a company called Cubemos and is no longer available. Alternative RealSense-compatible commercial skeleton tracking software ...