MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
I agree, the successful results with the official 1 meter cable would add to the likelihood of it being a USB cable issue. I would recommend not attempting further downgrades to older firmware at...
-
There does not seem to be a problem with the camera hardware as it is capable of streaming depth and RGB normally when firmware logging is enabled. A USB related issue with the computer's port or ...
-
Thanks very much, I look forward to your next report. In the meantime you could test whether it is possible to achieve a USB 3 camera connection with your current cable by going to the 'More' opt...
-
Hi Marcobsgallone 10 ft of cable length equates to around 3 meters. Because of the high volume of data that RealSense cameras can transmit, it is recommended that a high quality cable is used for...
-
It appears to be a web-browser related issue with the link rather than a problem with the article itself. It can be opened on Firefox, or opened in Chrome by right-clicking on the link and selecti...
-
Hi Agostino Gibaldi The unit of the RealSense IMU's gyro is radians per second (rad/sec), as verified in Intel's Getting IMU Data guide. https://www.intelrealsense.com/how-to-getting-imu-data-from-...
-
Hi Alexander Which version of the RealSense SDK are you using, please? And was it installed using the Intel.RealSense.SDK-Win10 automated installer file from the "Assets" file list of the SDK 'Rel...
-
Hi Daniel Sirkett The FSTROBE depth strobe signal is undocumented aside from the short 'Depth Strobe signal' reference in the data sheet for the 400 Series cameras. If you are aiming to generate...
-
It's no trouble at all :) The RealSense 400 Series camera models such as D435i do not support RS2_STREAM_POSE unfortunately. The pose stream is a feature of the RealSense T265 Tracking Camera m...
-
You could try disabling the RGB option Auto White Balance so that a manual value is used for white balance. A barcode will be sharper if the RGB Sharpness option is maximized to '100' Below are...