MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
All post-processing filters should be enabled by default except for these three: HDR Merge Filter By Sequence ID Hole Filling Filter Intel's post-processing filter guide at the link below lists t...
-
You are very welcome. It's excellent to hear that you achieved a solution. Thanks very much for the update!
-
After extensive testing with all Viewer options, I found that the best approaches were either to move the hand / arm a little further away from the camera or to switch to the D405 camera model, whi...
-
rs_sensor.h is not an SDK example program, but a file from the RealSense SDK that I quoted as a demonstration of code. Quoting code from the SDK's operating files is a useful way to illustrate use...
-
Hi Thomas Specte The official documentation for the rs2_set_intrinsics() SDK instruction is here: https://intelrealsense.github.io/librealsense/doxygen/rs__sensor_8h.html#ac1e8ebbd1e75fac3f1d7e9cc...
-
Update: the intelrealsense.com camera information pages are now accessible again. Thanks very much for your patience!
-
The Depth Units one is correct. The Disparity Shift option is three rows down from the arrow.
-
It's no bother at all. :) The D435i has a default minimum depth sensing distance of 0.1 meters / 10 cm, so if the hand / arm is nearer to the camera than 10 cm then the depth image will start to...
-
Hi Steve Steve If you are using Windows, could you try downloading and running the 2.49.0 version of the standalone RealSense Viewer - Intel.RealSense.Viewer.exe - and activating On-Chip calibrati...
-
Hi Steve Steve Apologies for the temporary intelrealsense.com site issues at the time of writing this. RealSense white-paper help guides are still accessible at the link below. https://dev.intelr...