MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Next, please try resetting the calibration of your camera to its factory-new default values using the instructions at the link below. https://github.com/IntelRealSense/librealsense/issues/10182#iss...
-
It has been confirmed to me that the D457 is not a USB "plug and play" camera and so cannot be used as a USB-only camera like other 400 Series models can.
-
Thank you. Please also try changing the Preset from 'Custom' to 'Medium Density' as this will provide a good balance between accuracy and the amount of depth detail on the image.
-
There is a high amount of variation of depth values in the same area, and some parts that have more distant depth than the others (when ideally the depth image of the flat wall should be all the sa...
-
Hello, please provide information about the questions below. 1. Which version of the RealSense SDK are you using? 2. Which firmware driver version does your camera have installed? You can fi...
-
Hi Fomalhaut92 By checking the source code of programs that make use of the large RealSense logo image, such as realsense-viewer and rs-software-device, I found that the image that they obtain is ...
-
Multiple .ply pointcloud files exported from the Viewer could be stitched together using a free open-source tool called CloudCompare (available on Linux via a Snap package if you do not have access...
-
Hi Yuval Arnon If you are able to compile computer code then the RealSense SDK's rs-kinfu C++ open-source example program may be helpful. It enables a single camera to be moved around a scene, pr...
-
Hi Matthew Derzay Have you made an ssh connection to the computer that you installed Yocto / librealsense2 on to test whether rs-server can be started (in case it was actually built). For example...
-
Hi Opdobro I hope that the information at the link below regarding the D435f's CLAREX NIR-75N filter will be helpful to you. https://support.intelrealsense.com/hc/en-us/community/posts/66577958049...