MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Makoto Terabayashi Yes, RealSense 400 Series cameras such as D435i can be used with USB 2. Are you attempting to connect to the camera using a program script that you have written yourself, plea...
-
If you are detecting the cameras automatically instead of manually specifying separate pipelines and serial numbers for each of the two cameras then I would recommend not attempting to alter the La...
-
With Raspberry Pi boards, only one RealSense camera per Pi board is usually used. Handling two cameras simultaneously may require a larger board, such as the Up Squared which can work with two cam...
-
Hi Surajkumar The Failed to set power state error suggests a problem with accessing the camera, either because it was already being used (i.e in a 'busy' state) or it is not being detected (perhap...
-
Hi Haris Sivic Not all of the RealSense Viewer tool's settings, like the ones that you quoted, can be exported to json file. An example of this is the Histogram Equalization depth visualization s...
-
Hi Jianfei Li The D415 has a rolling shutter on its depth and RGB sensors, whilst the D435 model has a rolling shutter on its RGB sensor but a fast global shutter for the depth sensor. If motion...
-
Hi Fomalhaut92 Advice about changing the logo image is provided in your other recent case at the link below. https://support.intelrealsense.com/hc/en-us/community/posts/10455990302611 One of the...
-
It looks as though the Yocto layer for librealsense uses the master branch of the librealsense GitHub, meaning that the latest version of librealsense should be installed. So your librealsense bui...
-
Update: the D457 is now listed as in stock at the RealSense Store. https://store.intelrealsense.com/buy-intel-realsense-depth-camera-d457.html
-
You are very welcome. It's great to hear that a calibration reset solved your depth value problem :)