MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The error message error 9986 intel streaming profile is not supported or configuration failed has not been previously reported. Instead of using version 2.12.0.0 of the Dynamic Calibration tool, ...
-
After the try_fetch fail, it found the camera on the next line of the log though.
-
I am not certain of the power draw of the SR300. However, when using a 400 Series camera model it has been recommended to budget for a power draw of 2 watts per camera, and the 400 Series is more ...
-
Okay, run the program again with the camera inserted. If the DCM program still does not detect the camera then it would suggest that there is insufficient power being supplied to the camera by th...
-
Let's try installing the Virtual Driver to see whether the driver being missing is the cause of your problem. Please remove the Depth and RGB drivers from the Device Manager again and unplug the c...
-
Can you check the camera privacy settings in Windows please to ensure that permission to access the camera hardware and permission for applications to access the camera are both set to On. Instruc...
-
Which RealSense camera model are you using, please? Also, which computer or computing board are you using (Raspberry Pi, Nvidia Jetson, desktop / laptop PC, etc). Can you provide an image of th...
-
Hi Mohammadmahmoodi8020 Please try resetting the calibration of your cameras to their factory-new default calibration in the RealSense Viewer tool with the instructions at the link below. https://...
-
Hi Icebean13 Don't worry, your English is very good. :) Have you installed the latest version of the SDK on Windows using the Intel.RealSense.SDK-WIN10 installer file in the 'Assets' file list ...
-
Hi Yinghaogo I tested my D405 on a scene where there was a small notch in an area of it for reliable positioning of the mouse cursor on the two streams. I was able to confirm the horizontal 5 pix...