MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
If you are using the RealSense ROS wrapper with your D455 then at the time of writing this the wrapper does not list official support for the D457 model, though a Pull Request (PR) has been created...
-
Hi Thermofluid06 The linked-to Intel de-serializer board product for use with the D457 camera model has the advantage of being able to be attached directly to an AGX Xavier computing board. You c...
-
Hi Dhongfhel Tare calibration improves the depth measurement accuracy of the camera. It may not be necessary for the D405 camera model though, as it is designed to provide high accuracy, high qua...
-
At this point we have tried everything that could be attempted to resolve a problem with launching the Dynamic Calibration tool and you have stated that it also occurs on several of your cameras an...
-
Let's try the previous 5.11.0.0 version of the Dynamic Calibration tool. I located a zip file for this version and uploaded it to Google Drive so that you can download the zip from there and extra...
-
Firmware 5.14.0.0 is the recommended firmware for use with SDK version 2.53.1 and there has been a report of an error when using 5.13.0.50 with 2.53.1. So I would recommend staying with your curre...
-
Thank you very much for your patience. Please next try downgrading your camera firmware from 5.14.0.0 to the previous version 5.13.0.50 to test whether there is an incompatibility with 5.14.0.0, w...
-
Thank you. Next, let's test for the possibility of a corrupted calibration table inside the camera, which can prevent the Dynamic Calibration tool from working when run. The calibration table can...
-
Although you are using a USB 3 connection, I wonder whether it is being mis-detected as USB 2.1. The Dynamic Calibration tool requires USB 3. If it was attempting to use a resolution of 1280x720 ...
-
You are very welcome. Thanks so much for the update!