MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
I will refer your question about whether a GMSL to USB convertor device can work with D457 to a team member of this Intel RealSense Help Center forum. Thanks very much for your patience.
-
My understanding is that the built-in IR projector's output is suitable for up to 2 m distance from the camera in darkness conditions, and that an IR illuminator would be recommendable if you neede...
-
Hi Roman Leuzinger The best technical discussions about use of an external IR illuminator with RealSense cameras are at the links below. https://github.com/IntelRealSense/librealsense/issues/1070 ...
-
The RGB sensor is not sold standalone, though it is my understanding from previous discussions on the subject that sensor modules that meet the MIPI CS-2 interface format should be compatible. Re...
-
In regard to modules with an RGB sensor, the D415 model of Depth Module has an integrated RGB sensor on its PCB. The D401 Depth Module has RGB without an RGB sensor, as it can output high qualit...
-
Hi Roman Leuzinger The D430 is a caseless Depth Module that is not equipped with an RGB sensor. When the D430 is used in the cased RealSense D435 and D435i models, the RGB sensor is connected sep...
-
Hi Roman Leuzinger Although the D457 has a USB port, it is intended for use in debugging or production line testing and the camera should be used with a GMSL FAKRA cable. A 1000 mm / 1 m cable is...
-
The D405 / D401 is not able to see infrared frequencies due to a blocking IR Cut filter on its lenses. So it would not be suited to complete darkness unless it is possible to provide short-range v...
-
Hi 90reza The links below that relate to looping through multiple bag files will hopefully be of use to you. https://github.com/IntelRealSense/librealsense/issues/6340 https://github.com/IntelReal...
-
If changing camera model is an option then using the D405 model may provide better results, as it is designed for high accuracy, high quality images at close range (7 cm to 50 cm). If you need...