MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
By default, the Windows version of the RealSense SDK uses Windows Media Foundation as its backend. So if the preset changing problem is caused by an error with Media Foundation's MFCreateDeviceSou...
-
Are you using Windows, please? There was a case in 2019 of the Viewer freezing when changing the preset and it was thought to be caused by the 'build' version of Windows that was being used and no...
-
This question is replied to at the link below. https://support.intelrealsense.com/hc/en-us/community/posts/15623819649299
-
RealSense can run on low-end computers and computing devices. The camera also contains hardware that performs graphics processing so that having a good graphics card in the computer is not a requi...
-
Are you trying to write your own program script, please? If you are then which programming language are you using (C++, C~ or Python) and what are you aiming for your program to do, please? If y...
-
Yes, RealSense can use multiple camera (two or more). An easy way to test this is to use the free RealSense Viewer tool and add additional cameras using the Add Source button at the top of the Vie...
-
Hi Jomanaashraf8 The term '3D reconstruction' usually refers to capturing a depth image of a scene, like the scene of outdoor trees in the RealSense depth image below, and saving it to a file. Is...
-
Hi Zhaniyarnurlan Although the ethernet networking system that you linked to supports 1280x720 at 6 FPS, the D455 camera model does not support it as its minimum FPS speed is 5 FPS instead of 6 an...
-
It's an infrared based laser. If you look at an infrared image, surfaces in close range to the camera are strongly illuminated when the projection is enabled but you do not see that surface visibl...
-
As long as IR light can still pass unobscured through the overlaid CLAREX filter after the anti-reflective coating is applied to it then I would think that it would be okay.