MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Avensc If the camera works normally until the drone is started and the camera is mounted on the drone, could you first check please whether severe vibration is being transmitted from the drone'...
-
Hi Mau Have you tried using the L515's USB cable with the D455 to confirm whether the problem is with the D455's cable, please? If the D455 is using the USB C to C cable, using a C to C cable wi...
-
Hi Siyuanwu99 Do you know which version your Vision Processor D4 board is, please? There are 4 versions - V1 to V4 - and most only work with a specific Depth Module model. A D410 will be compati...
-
Hi there! Yes, the Dynamic Calibration tool is compatible with the RealSense D405 camera model.
-
Problems with the depth image can often be compensated for with changes to settings. Would it be possible to provide an RGB color picture of the scene that you are capturing as a point cloud so I ...
-
The camera will capture the areas of the scene that are inside its field of view size, so a single camera may not be able to fit an entire row of trees within its view without moving the camera. I...
-
The link below highlights the section of the ROS2 wrapper's base_realsense_node.cpp file that handles diagnostics publishing, including temperature. https://github.com/IntelRealSense/realsense-ros/...
-
Hi Jesus Dovale There is not such a list available for the /diagnostics topic. The only contents of the topic referred to in the ROS2 wrapper's release notes are frequency monitoring and ASIC & pr...
-
There are also many official guide articles at the link below. I cannot link to it from this page, so please type the address below into your browser.
-
There is a large range of videos at the official RealSense YouTube channel. https://www.youtube.com/@IntelRealSense/videos