MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
You could use an Ubuntu system monitoring tool such as htop to see how the system is reacting.
-
RealSense 400 Series camera such as D455 are used widely in commercial and industrial applications, including critical ones. When problems do occur, we endeavour to help the customer to find solut...
-
You are very welcome. It's great news that you were able to correct the problem. Thanks very much for the update!
-
It's great to hear that you achieved a solution. Thanks very much for the update!
-
USB stability should improve if the build flag -DFORCE_RSUSB_BACKEND=true is used, as this bypasses the kernel and so you would not need to take the kernel into account. An RSUSB = true build is n...
-
Is /diagnostics not on the topics list that is produced if you input ros2 topic list
-
As your script works normally when the drone process is not running, it does not seem as though there is a problem with your RealSense code. However, it may be worth starting the drone and then ru...
-
It's no problem at all. Did you purchase the 8-pack of D450 and D4 V3 on the RealSense Store or buy one of each individually from another retailer, please? Are you able to perform a firmware upd...
-
Hi Agan Simsek Installation of the librealsense SDK and the RealSense ROS wrapper on Raspberry Pi can have significantly more problems than with Nvidia Jetson or x86 / x64. So if you have the cho...
-
The camera should definitely not be consuming 170% of the CPU's usage. For two simultaneous streams (depth and color), 70% would be a more reasonable expectation. I would be concerned if the over...