MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Tsubota Kazuhiro Thanks very much for your questions. 1. Yes, you can modify the queue size using the RS2_OPTION_FRAMES_QUEUE_SIZE instruction. By default the queue can circulate 16 frames ...
-
One way to mute that message specifically may be to remove the 'if' check for all types of control_transfer returned warnings by commenting line 42 of the source code of the SDK file messenger-libu...
-
If a window covered the projector then there would be a risk of the projector's laser reflecting and scattering, as advised by a RealSense team member at the link below. https://github.com/IntelRea...
-
As the settings do not affect each other but they all independently increase brightness, it should not matter which one is changed first.
-
Hi Tsubota Kazuhiro In terms of RGB, exposure, gain and brightness will all affect the brightness level of the image. There is not a relationship between them though in the sense that changing on...
-
Hi Roman Leuzinger Typically in this situation, defining a logging level to exclude certain categories of messages from the log will be the solution. The 'Resource temporarily available' message ...
-
Hi Roman Leuzinger The filter on the D435f and D435if (a D435i with filter) blocks visible light frequencies whilst allowing near-infrared frequencies to enter the sensor. It is not an IR-Cut fil...
-
There is not any data or past-case references available regarding RGB performance at very high temperature. My expectation is based simply on how an RGB image typically remains stable even when ot...
-
Hi Yixun Liu The MFCreateDeviceSource error in the log suggests that Windows cannot access the camera. If the camera works normally on another PC then the error may be being caused by the Windows...
-
Hi Grace There is a relationship between the operating temperature and the temperature of the camera's outer casing. Intel lab tests found that if the external casing temperature is below 44 degr...