MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
I recommend using at least RealSense SDK version 2.35.2. This is because Jetsons had problems with multi camera setups, and SDK 2.35.2 introduced improvements to multicam support. RealSense camera...
-
Hi Avino1033 The new RealSense D455 has a fast "global shutter" on its RGB sensor for the first time to match the fast global shutter on the depth. So if your project will use RGB color, then the...
-
The filtered images look good, bearing in mind the resolution being used. Thanks for sharing your results in detail so that others can benefit from the knowledge. Regarding a Python timer for savi...
-
Hi Yehtet4utycc If the location that the camera is being used in has fluorescent lights such as ceiling strip-lights then they can flicker at frequencies that are hard to see with the human eye an...
-
The firmware driver in the camera can make decisions about which model the camera is based on the internal sensor components that it can detect. For example, if the firmware cannot detect the D435...
-
Hi B Raemaekers D435i is not currently supported on Windows 7, unfortunately.
-
Firmware version 5.12.5.0 has been available since yesterday. It is not available as an individual download on the firmware releases page yet at the time of writing this message but can be updated...
-
I'd be grateful if you could provide answers for the questions below, please. - Do you get any frames if you use 30 FPS instead of 15? - Are you using the official short cable supplied with the c...
-
The 6th generation of Intel processors dates from around early 2016. Intel processors are up to 10th generation now at the time of writing this in 2020. When Intel processor generations are menti...
-
You're very welcome! In answer to your new questions: 1. Regarding questions about the Coded Light patterns, I will refer you to the guidance of a guy called Samontab who was an expert on the sub...