MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
If the large removable cap on the side of the camera that covers the blue GMSL connector is removed by pulling it sideways away from the camera then there are two small screws either side of the co...
-
Another D457 user had the same non-detection problem as you in March 2023 when installing an old firmware. https://support.intelrealsense.com/hc/en-us/community/posts/15226169805971/comments/152268...
-
Hi Collins Lu Such a report is not available. However, RealSense 400 Series cameras can operate indefinitely so long as they remain within their recommended operating temperature range. If a ca...
-
If the Windows USB sound effect is heard when the camera is unplugged and re-inserted then this suggests that the camera's drivers will at least be detected as D455 in the Cameras section of the Wi...
-
Since support for D457 was introduced in SDK 2.53.1, it may be best to return to that SDK. If you visit the link below and download and run the Intel.RealSense.SDK-WIN10 installer file in the 'Ass...
-
When the mode switch was moved to the MIPI position, is it possible that it was not moved back to the USB position despite the attempt to do so? It can be difficult to tell which position the swit...
-
Hi Lucas I recommend first trying the repeating of the rs-fw-update command but removing the -r command that checks for cameras that are in recovery mode, as it is possible that the camera is not ...
-
Hi Jim, if you are using the D457 with a USB cable then you first need to move a physical hidden switch on the casing to the 'USB' position using the instructions at the link below. Have you done ...
-
Hi Maoshouyun Support for the D457 camera model was added to the ros2-development RealSense ROS2 wrapper at the start of 2023. https://github.com/IntelRealSense/realsense-ros/pull/2557 Updates o...
-
Hi Pedrovigano1997 The official information page for the RealSense D435f camera model highlights depth noise quality and improved range as the primary advantages of the filter. https://www.intelre...