MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Tsubota Kazuhiro Global Time should be disabled for individual sensors, as advised at the link below. https://github.com/IntelRealSense/librealsense/issues/6195#issuecomment-610199258 Here is...
-
The built-in laser of RealSense cameras is low intensity at a default power value of 150mW and would not penetrate through layers of body fat to reach a baby inside. By pre-term though I assume yo...
-
Hi Roberto Mangano The SR300 is no longer available and is out of stock at most of the major online suppliers of RealSense products. The only stockist I could find that lists the SR300 Depth Mod...
-
Hello, if you are using the RealSense Viewer tool then it is likely that the 4 meter depth range limit is because a post-processing filter called Threshold Filter is enabled. If you go to the St...
-
Hi Ricky Sato I have not previously seen a case with a similar ground loop. Instead of using ordinary plastic screws though, perhaps a non-conductive screw with strength as strong as metal screws...
-
The advice was to connect the older version of the D450 depth module, yes. If you do not already own an older K83121-100 version of the D450 module though then as far as I am aware it is not poss...
-
Yes, another RealSense customer at the link below had their D4 board identified as D405i Tester when it was disconnected and they were performing a firmware update with the depth module unplugged. ...
-
Regarding your removed message about using the command .\rs-fw-update -f Signed_Image_UVC_5_14_0_0.bin you should not need to put .\ in front of rs-firmware update, and just input rs-fw-update -f ...
-
If you need to use the camera in USB 2.1 mode instead of USB 3, please try unplugging the micro-sized end of the USB cable from the base of the camera, turning it around the opposite direction and ...
-
There is not documentation for the procedure but it should be relatively straightforward. 1. Open up the casing. 2. There are two main modules inside the casing, the Vision Processor D4 V5 (w...