MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Up202109482 The mathematics is a little complicated. RealSense 400 Series depth cameras such as D455 represent their depth as 16-bit uint16_t 'pixel depth' values which have a minimum-maximum ...
-
Hi John Swensen The L-shape adaptor part is not available for separate purchase, unfortunately. I researched possible alternative adaptor parts but most would not fit in the space of the original...
-
Hi Yassine Rahrah Could you first try unplugging the micro-sized end of the USB cable from the D457 camera, reversing the connector's orientation and plugging it back into the camera, please (USB...
-
Hi Dlagunes If you need to depth sense at up to 20 m then the RealSense D455 camera model can meet your requirement. Its infrared and RGB sensors can see further than that. https://store.intelrea...
-
Translation: Humanoid Camera SelectionWhat are the general functional requirements of a humanoid robotHow to choose a depth camera based on these requirementsUnder what circumstances do you need t...
-
Hi Yadavashwani467 Do you have access to the RealSense Viewer tool? If you do then you can test playback of your bag to see whether the file itself is okay by dragging and dropping the bag file i...
-
It sounds as though the entire camera is not being detected on Nano, not just the camera's IMU. As the camera can be detected on Windows, we can assume that the camera hardware, USB cable and came...
-
Are you using Oracle VM VirtualBox on the Nano?
-
Does your model of Jetson Nano have a barrel jack connector for providing extra power? If your Nsno does have one then Intel strongly recommend enabling it using the instructions at the link below...
-
Are you able to use the realsense-viewer tool? If you are, is the camera detected in it and can you use the IMU by enabling the Motion Module in the options side-panel?