MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Ihyunp1113 It could be an issue with the USB controllers that this particular PC uses. The ports on a PC are handled by a USB controller, typically with one controller for each port. The cont...
-
You are very welcome. I look forward to your next report. No, I have not used multicam with a USB2 hub.
-
You could also try linking your existing hubs together and dividing the cameras across them (such as 2 on each hub). The USB standard allows up to 5 hubs to be 'daisy-chained' together on the same...
-
Hi Deepak Kumar In Intel's multiple camera white-paper document they tested up to 4 cameras with the AmazonBasics powered USB3 model. I used an AmazonBasics hub myself with RealSense cameras base...
-
Hi Cem Girit Whilst the default minimum depth sensing range of the D405 camera model is 7 cm, it can be reduced as low as 4 cm using a setting called Disparity Shift. In regards to your question...
-
-
RealSense cameras can be placed inside a custom-built protective housing in very extreme environments, such as the example below.
-
For use in all weathers outdoors, the D457 model may suit your needs best as it has IP65 rating that protects it from dust and water entry.
-
If the ambient temperature was sub-zero then the internal operating temperature would likely not be as low as the outer environment because of the heat generated from the electronics. Maximizing t...
-
Laser shut-off does not prevent the camera from operating, though the infrared image will likely be darker and the camera would not be able to provide an infrared image at night unless an external ...