MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi F Ricardo Auto With RealSense cameras that have front glass, depth is measured from the glass and not at the lenses. You can subtract 3.7 mm from the depth value to find the ground truth depth...
-
The link below has Python scripting for changing the depth scale with the instruction rs.option.depth_units https://github.com/IntelRealSense/librealsense/issues/10976#issuecomment-1271236193
-
The company autoVimation (who manufacture RealSense camera enclosures) also have a non-RealSense waterproof enclosure that can fit a 61x61 mm sized camera. The only product in the RealSense range ...
-
The discussion at the link below is relevant to your concerns. https://support.intelrealsense.com/hc/en-us/community/posts/16763918575379-D457-Waterproof-USB-C-connection Once underwater, the cam...
-
Hi Ali Rohan2003 Unfortunately it cannot be purchased as it was custom-made by the people who developed that particular underwater project. The D457 camera model has an IP65 rated casing that pr...
-
Hi Javier The built-in projector is a separate component from the infrared sensors and projects a semi-random dot pattern onto the surfaces of objects in the real-world scene to aid the camera in ...
-
Thanks very much for the clarification. You can customize the scale that depth measurements are reported in by changing the depth scale option. By default on D405, depth is reported in the centi...
-
RealSense cameras have a minimum depth sensing distance, below which depth data breaks up and then disappears. By default on D405 this minimum distance is 7 cm, so the depth image will only contai...
-
The details of RealSense stereo algorithms are not open-source publicly available information, unfortunately. Intel have another introductory depth guide that discusses stereo depth principles a...
-
Hi Dimouzoi There is limited information available about how RealSense cameras calculate a depth frame. The best available quote is on page 16 of the data sheet document for the RealSense 400 Ser...