MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Fulvio Diluzio RealSense cameras equipped with an IMU can use a Python-based tool to calibrate the IMU by proceeding through a six stage process where the camera is placed in different rotation...
-
Hi Shabouza030 RealSense cameras that can track orientation do not have a magnetometer. They are instead equipped with an IMU component containing a gyroscope and an accelerometer. There have...
-
Hi Gatordevin Yes, it is fine to update the firmware of the D457 in the RealSense Viewer's firmware update function under the More option when the camera is detected as D455 in USB mode. RealSen...
-
Hi Martino Lorusso The RealSense SDK's open-source rs-kinfu C++ / OpenCV tool may meet your requirements. It uses frame fusion to progressively build up a point cloud image with a single camera. ...
-
That configuration should be supported when the camera is on a USB 3 connection. If the USB connection was being detected as the slower USB 2.1 though then it would not be available. Instead, the...
-
Hi Kai Chen2 The 'Cannot resolve requests' error usually means that a stream resolution / FPS configuration has been requested that the camera cannot provide. Which resolution and FPS is your prog...
-
Thank you for the data. Are you using the official 1 meter long USB cable supplied with the camera or a longer USB cable of your own choice, please?
-
Aside from the mentioned Nvidia Jetson and Up SBC boards that are known to work with two RealSense cameras (and also Intel NUC computing products), it is difficult to provide recommendations for sp...
-
Hi Chandiran When you mention 'dual sensor', do you mean two separate cameras (the D410 and another camera). If so then Raspberry Pi single-board computers usually have only one RealSense camera ...
-
Hi Sundaramoorthi S The number of RealSense cameras that a single-board computer can support simultaneously will depend on the board's hardware specification. Raspberry Pi is best suited to one c...