MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
RS2_OPTION_MIN_DISTANCE is different from Disparity Shift, as it sets the minimum depth distance in meters to be rendered on the depth image. The ball would still become undetected though if it mo...
-
The distance from the front glass.
-
Hi Wmaass88 When tracking fast motion of small objects, the higher the FPS speed used the better. Could you try using 90 FPS if you are not doing so already, please? If your software applicatio...
-
The above image originates from the Intel guide linked to below. https://www.intelrealsense.com/best-known-methods-for-optimal-camera-performance-over-lifetime/#3.6.3 The image in the guide direc...
-
You could try the Ubuntu MATE OS. https://dev.intelrealsense.com/docs/using-depth-camera-with-raspberry-pi-3
-
Hi Matt There is not a CAD file available for the OEM calibration target product, unfortunately. There is also not a CAD file for the FRAMOS D415e industrial RealSense camera, as it is a product ...
-
The fx and fy fields describe the focal length of the image, as a multiple of pixel width and height. The ppx and ppy fields describe the pixel coordinates of the principal point (center of projec...
-
As shown by rs-enumerate-devices -c, each resolution has different intrinsics. Unless you define your own stream configurations with cfg instructions, a program will use the default stream profil...
-
A RealSense user at the link below who also has a Raspberry Pi is currently experiencing the control_transfer returned and the Frame received with streaming inactive,Depth0 error with Ubuntu too (W...
-
Are you able to stream depth when these errors and warnings are appearing in the log, or is there no depth stream?