MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
When the emitter is enabled, a built-in projector component in the camera casts a pattern of dots onto surfaces in front of it. This pattern is invisible to humans but can be seen by the camera. ...
-
Hello, if the wall is plain with little or no texture on it, and especially if its color is white, then the camera will have difficulty analyzing it for depth information when placed at a distance ...
-
Hi Brattlirannin Advice about resolving this issue can be found at the link below. https://github.com/IntelRealSense/librealsense/issues/11789
-
This question has been replied to at the link below. Thanks! https://support.intelrealsense.com/hc/en-us/community/posts/4548413451539/comments/25364882859795
-
A RealSense user at the link below reported successful use of a D435 camera on an M2 Mac. https://github.com/IntelRealSense/librealsense/issues/11815#issuecomment-1609152575
-
Hi Caixadomiguel At the time of writing this it is still rare for RealSense to be used with M2 Macs. The link below has a guide for installing RealSense for use with TouchDesigner on an M1 Mac th...
-
You are very welcome!
-
RealSense has a High Dynamic Range mode where auto-exposure is disabled and the camera can instead alternate between two different exposure values so that it can cope with both light and dark regio...
-
If you have the Stereo Module enabled at the same time as RGB then I would suspect that the infrared dot pattern is leaking through to the RGB image. This is not meant to happen and is a highly ra...
-
Hi,a response to this question has been posted at the link below. Thanks! https://github.com/IntelRealSense/librealsense/issues/12574