MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Juan Diezyanguas I must emphasize that my C# programming knowledge is limited, though I will do my best to be of assistance. In regard to creating multiple contexts, at the link below a RealS...
-
Information about how the pre-made Raspberry Pi network-equipped SDK image is not available. In addition, networking support was removed from the SDK in version 2.54.1 onwards. This means that the...
-
Hi Juan Diezyanguas A RealSense user at the link below replaced the RTSP protocol with ROS networking protocols. https://github.com/IntelRealSense/librealsense/issues/6841#issuecomment-660859774 ...
-
I look forward to your next update. Good luck!
-
Possibly you have two versions of librealsense (2.54.1 and 2.54.2) installed on your computer. Whilst this is not ideal as different installations of librealsense can conflict, if you do have two ...
-
848x480 is the optimal resolution for depth accuracy on most RealSense 400 Series camera models including D405, but using 1280x720 should not significantly impact accuracy and so it should be fine ...
-
Hi Toni Divic I have not seen that particular warning message before. Which version of the RealSense ROS2 wrapper are you using, please? The appropriate librealsense SDK and RealSense ROS wrap...
-
When the wait_for_frames() instruction is used, the RealSense SDK will attempt to find the best match between the depth and color sensors. https://github.com/IntelRealSense/librealsense/issues/1548...
-
Hello, there is an example of a Python script at the link below for defining and applying post-processing filters, including the Temporal filter. https://github.com/IntelRealSense/librealsense/issu...
-
Hi Jhheo When the firmware driver detects that the Projector temperature of the camera has dropped below 0 degrees C then the projector's laser will shut off. It also shuts off if the Projector t...