MartyG

  • Total activity 5964
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 7 users
  • Votes 3
  • Subscriptions 1820

Comments

Recent activity by MartyG Recent activity Votes
  • You only need to use an index number for infrared if you are streaming both left and right infrared.  In that case, left infrared is '1' and right infrared is '2'.  For left infrared only, you can ...

  • Hi Yixun Liu  Thanks very much for your questions.   1.  Only the left infrared sensor can provide an RGB color image.  The right infrared sensor is monochrome.   2.  You can stream the depth image...

  • It does not have to be the original model of UP board.  Another board in the current UP range or a similar 'x86' architecture board such as Lattepanda should be fine.   The 'depth camera over ether...

  • Thanks for the reminder about the OnDevicesChanged function in C#.   If you have one context and multiple cameras attached then you should be able to access individual cameras by their serial numbe...

  • When a function is labelled as deprecated it means that while that function is currently supported, it may be removed in the future and it is recommended that an alternative function is used instea...

  • Factors visible in the RGB scene that could affect depth accuracy include natural lighting (facing the camera directly towards the sun), artificial lighting (such as fluorescent ceiling strip light...

  • The filter smooth alpha setting slows down the rate at which the image is updated,  So whilst it can stabilize depth fluctuations, it can also cause a visible delay in responding to movement of the...

  • The RealSense SDK's bag files store raw data and they do not store aligned data, only the individual streams.   As a bag file does not store filtered data, a depth stream stored in it will be the r...

  • To stabilize fluctuating depth values using the temporal filter, its filter smooth alpha setting should be configured.  By default its value is '0.4', but data should fluctuate less if it is change...

  • Hi Teschkec  The D435i camera model lacks the in-built ability of the T265 Tracking Camera model to know the camera's position and rotation (its pose stream), or to analyze the pose of objects obse...