MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The D455 camera model requires a minimum of firmware 5.13.0.50. Firmwares older than this should not be installed in a D455-type camera. Cameras that are identified as a D456 need a minimum of...
-
Intel have a YouTube video guide at the link below for building RealSense body joint tracking from scratch. https://www.youtube.com/watch?v=VSHDyUXSNqY
-
Hi Sohwa427 There is no RealSense camera model that can stream RGB from both the left and right infrared sensors. Only the left sensor supports an RGB stream, and this feature is available on the...
-
That is correct, the raw infrared frames used to calculate depth are unrectified. In regard to the infrared streams, Y8 is rectified and Y16 is unrectified because it is used for camera calibration.
-
D457 supports two types of cable connection, GMSL / FAKRA (a high speed connection used in the automotive industry) or USB. By default the D457 operates in GMSL / FAKRA mode and is detected as a D...
-
Hi Dafni Xanthopoulou When new RealSense camera models are introduced and they are detected as having a new model number that has not been used in the past, support for those models is not backdat...
-
Hi Niha K Cse Which RealSense camera model are you using, please? The metadata message may be appearing because support for camera metadata is not enabled. You can test whether it is enabled by...
-
Please ignore the above link. It is a game advert.
-
Hi Surajbalore888 Measuring between two points on the same image instead of between the camera and a point may enable you to meet your goal. C++ https://github.com/IntelRealSense/librealsense/tree/...
-
Please do not click on the link in the comment above. It is an advert for a game.