MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The reason why the chair would be inaccurate is clear then. Plain white surfaces (such as white walls) can also be difficult for the camera to analyze. You could try increasing the Laser Power op...
-
Hi Jinuk Yoon High temperature should not be a cause of USB connection loss. There may be some problems with the image above 42 degrees C, and once the Projector Temperature is 60 degrees or abo...
-
Are the desk or chair dark grey or black in color? If they are then this can cause depth to be missing or highly inaccurate. This is because it is a general physics principle (not specific to Rea...
-
The old support thread regarding lens removal is below, though it does not provide details about the procedure that was used to do so. https://community.intel.com/t5/Items-with-no-label/Realsense-C...
-
Hi Subscriptions Official updates for Mac support in the RealSense SDK ceased after MacOS High Sierra in 2018. However, RealSense cameras have continued to work with Macs in subsequent MacOS rele...
-
Catalina and Big Sur were the most reliable MacOS versions before Monterey, which came after Big Sur. Monterey was when problems with RealSense compatibility started becoming more common.
-
Hi Jhheo The field of view of the image will vary depending on which resolution is selected. The smaller the resolution, the more restricted the view of the scene will be. So you can affect the ...
-
If the image freezes or severely deteriorates in quality but the recovers after the camera is moved or covered over with the hand then this can be symptomatic of the camera having been faced direct...
-
Infrared should be available on both a USB and a GMSL / FAKRA cable connection. A plugin will only be able to display a particular stream type if it is designed to do so. For example, a plugin m...
-
Hi Kawasyuuqq Do you experience similar problems if you test the Python keypress capture script at the link below, please? https://github.com/IntelRealSense/librealsense/issues/8388#issuecomment-7...