kris gunnarsson

  • Total activity 6
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 2

Posts

Recent activity by kris gunnarsson Recent activity Votes
  • Hole in depth image of a D435

    Hello, again. I am attaching an image from a D435 that shows both an RGB and z-clipped (0.25m-3.0m) depth image. The D435 is mounted about 6" off the deck and tilted about 16 degrees down toward th...

  • Tale of two D435's or bad depth image

    I have two (2) D435 cameras that I have set up to give depth of the same scene. I am using intel-relasense-viewer to capture depth images. I have done a hardware reset on both attempting to put the...