kris gunnarsson
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by kris gunnarsson-
kris gunnarsson created a post,
Hole in depth image of a D435
Hello, again. I am attaching an image from a D435 that shows both an RGB and z-clipped (0.25m-3.0m) depth image. The D435 is mounted about 6" off the deck and tilted about 16 degrees down toward th...
-
kris gunnarsson commented,
Per your suggestion MartyG, I calibrated the camera and here are the results. This looks very good. The ease of use of the dynamic calibration application was excellent. Good stuff! Thank you.
-
kris gunnarsson commented,
A-ha! I had thought about calibration but this far out of whack I thought that might do little. There's probably a thin line between in and out of calibration. The team thinks heat is unlikely but ...
-
kris gunnarsson created a post,
Tale of two D435's or bad depth image
I have two (2) D435 cameras that I have set up to give depth of the same scene. I am using intel-relasense-viewer to capture depth images. I have done a hardware reset on both attempting to put the...