Daniel Rehak Ext
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 3
Activity overview
Latest activity by Daniel Rehak Ext-
Daniel Rehak Ext created a post,
Intel® RealSense™ Depth Module D450 - maximum current drawn
Hello, I want to ask whether there is a state where D450 module can draw more current - for example if some sort of fault occurs. Documentation states that for 5V it will draw 700mA (source: datash...
-
Daniel Rehak Ext created a post,
Intel® RealSense™ Tracking Camera T265 - max current drawn in fault state
Hello, I want to ask whether there is a state where T265 camera can draw more current - for example if some sort of fault occurs. Documentation states that for 5V it will draw 300mA (source: datash...
-
Daniel Rehak Ext created a post,
D400 and D450 end of life
Hi, I could not find this information anywhere so I ask here: when is end of life of products D450 and D455? By end of life I mean end of production and end of selling them.