405275935

  • Total activity 5
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by 405275935
  • 405275935 commented,

    thanks,problems is solved by copying those files: pyrealsense2.cpython-310-aarch64-linux-gnu.so,pyrealsense2.cpython-310-aarch64-linux-gnu.so.2.55,pyrealsense2.cpython-310-aarch64-linux-gnu.so.2.55...

  • 405275935 commented,

    it doesn't work,you can see ,under the pyrealsense2 is  pyrsutils.cpython-310-aarch64-linux-gnu.so,it maybe wrong.

  • 405275935 commented,

    Yes, I recompiled and reinstalled pyrealsense2. However, when running , the error "module has no attribute 'pipeline'" appears.rs.pipeline()

  • 405275935 created a post,

    D455 is not detected in python code

    Hardware: RK3588, system Ubuntu 20.04, kernel 5.10.16. During the installation of Intel RealSense SDK 2.0, I encountered an issue where the kernel version was not supported. Therefore, I used the l...