Alberto Biencinto
- Total activity 7
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Posts
Recent activity by Alberto Biencinto-
Camera D415 24h working.... capable?
I'm using this camera on my work, it's always analizing frames with Opencv an Ros2. Is this camera ready to be all time running ? At this moment the temp don't get warm so i think it's ok for alway...
-
Usb 2.0 in Jetson Orin, not 3.2, why!
Hi! I'm using the Jetson Orin Nano and D415 on my proyect. The cam works right except with the conection, i'm using the inbox USB 3.2 Cable connected to the Jetson Orin witch is USB 3.2 capable. Bu...