Liam Neric

  • Total activity 13
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 5

Posts

Recent activity by Liam Neric Recent activity Votes
  • Resetting Cache, Realsense-Viewer

    Hello, we have noticed that sometimes when the camera loses connection, the only way of resetting is running the realsense-viewer. We wonder what kind of camera/usb resets are done during start-up,...

  • Overwriting D400 camera Intrinsics

    Is there any way of overwriting the camera intrinsics (with my own calibrated intrinsics) for the RGB camera, specifically for the D455, preferably by realsense C++ or Python API? Is it possible th...

  • Quality of OEM Calibration Tool

    Hello Intel support and MartyG. We are considering purchasing the OEM calibration target. Are there any guarantees regarding accuracy for the RGB calibration? It would be disappointing if it under-...

  • D455 RGB streaming

    Hello, I want to stream the RGB camera of my D455 to a screen using MJPEG. I have managed to do this previously with the D415, specifying yuv422 as the pixel format and 1280x720 as resolution. But ...

  • D455 Poor depth quality

    I have evaluated two different units of the D455 camera to calculate the depth to the surface of a small cylinder as a test (see middle of depth images). I get a 55mm error at 2m distance, and simi...