Coltongcunningham

  • Total activity 6
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Coltongcunningham
  • Coltongcunningham commented,

    Thank you Marty, that is really helpful. Another question, what do people usally do to increase the resolution of the camera with far away objects? Because the camera is able to sense up to 6 meter...

  • Coltongcunningham commented,

    One more question, I see in the viewer, that I can change the maximum detectable distance, and the minimum detectable distance. However, when I look in the .json file settings, I don't see an optio...

  • Coltongcunningham commented,

    Hi, I just tried that, and it worked I believe. I attached the code I used to load in a .json file and then load those settings into the intel camera incase it is helpful for others down the road. ...

  • Coltongcunningham commented,

    Hi Marty, Thank you for your response. I think loading in a .json file would be a good solution, but I think there is an issue with the Matlab wrapper code. I a getting the same error as seen in th...

  • Coltongcunningham created a post,

    Realsense D457 Zoom and settings adjustment

    Hello,  I am using the intel real sense camera for an orange detection robot. I have researched the camera from other threads, and it seems that the camera can only zoom through digital zoom. This ...