Sasabukreev808
- Total activity 9
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 3
Posts
Recent activity by Sasabukreev808-
Question about microcircuit
The mircocircuit has two fields where you can connect a camera. Do I understand correctly that one of them is used for debugging, and the other is used for normal purposes?
-
Camera shows frames only in realsense-viewer and only if „Enable hardware logs” option is turned on
Hello! I have encountered a problem when i wanted to add a camera to my project. It shows me frames only in Intel's special program and only when i turn on “Enable hardware logs” in general logs zo...
-
Frames didn't arrive in 5 seconds
Hello! I have encountered an issue: my program haven't received any frames from the camera Intel RealSense Depth Module D410. The same problem is in the realsense-viewer. What can cause this troubl...