2935253854

  • Total activity 6
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 2

Posts

Recent activity by 2935253854 Recent activity Votes
  • crop the .bag file

    I used the D415 camera to record a bag file, but I only need the video recording after 5s of the file, is there a way to crop the file

  • D415 gets the real distance

    When the D415 camera acquires the real distance, does it need to perform operations such as camera calibration, color map and depth map alignment, or can it directly use the get_distance(x,y) funct...